GRUNDFOS CEO WATER MANDATE 2015 GRUNDFOS CEO WATER MANDATE 2015 Grundfos pumps keep water at bay When rising waters turn into a flood, the consequences can be severe and sometimes claim lives. However, the risks can be brought under control to ensure the safety of people living along the shoreline. From Semarang, Indonesia to Louisville, USA Excessive water can be very damaging if it is not controlled. The port city of Semarang in Indonesia is home of two million people and is a bustling centre of trade. The low-lying city is wedged between the ocean and mountains, making it vulnerable to floods. These floods can be devastating for residents and cause damage to both homes and businesses. Meanwhile, residents of Louisville in the US state of Kentucky are also familiar with the danger of flooding. Although the neighbouring Ohio River is a source of life and a gateway for commerce, it also has the power to cause catastrophic disasters. Pumps with plenty of muscle Thanks to cooperation between local and global institutions, a new pumping station (complete with Grundfos pumps) has been implemented successfully in Semarang making the city better equipped to manage flood risks. The project is beneficial for Grundfos in two ways. Firstly it is good business, and secondly it is in line with The Grundfos Purpose- “contributing to global sustainability by pioneering technologies that improve quality of life for people and care for the planet”. Managing Director for Grundfos Indonesia, Gert Borrits, says: “This project has been very important for us because we have been able to make a difference for our fellow citizens through our work and solutions”. In Louisville, Grundfos has also played a major part by working closely with local operators to ensure pumping stations are functioning well. A new pumping station, consisting of Grundfos Peerless pumps with a combined pumping capacity of 3.8 million litres of water per-minute, helps to manage water levels and protect homes and businesses. These projects require close collaboration and knowledge-sharing to succeed in protecting and improving water management.
Download PDF file
Cookie policy