GRUNDFOS INDUSTRY CR 95 - CR 155 GRUNDFOS CR 95 - CR 155 FOR ENGINEERS WHO LIKE TO MOVE THE LIMITS The new generation of Grundfos CR pumps introduces world-class efficiency upgrades and a range of new features that will further improve pump reliability. More reliable The new generation of large CR pumps has been made even more robust than its forerunners through use of state-of-the-art technology in simulation-design, materials, testing and production. And with the addition of predictive monitoring, the new Grundfos CRs will become virtually unstoppable. More cost-efficient With its optimised hydraulic design - from impeller and guide vanes to inlet, discharge port, sleeve and diffuser - the new generation of Grundfos CR offers world class energy efficiency. Due to its small footprint, it is much easier and less costly to install than other pump designs. More options The new generation adds even more options to what was already the most modular pump program in the world - including higher pressure, lower NPSH and the use of standard motors. And of course, the new CRs are also available as combined systems with dedicated CUE frequency converter and as boosters systems.
Download PDF file
Cookie policy