7. Existing User: Log in and Tap: ” Add New” (Top Right in home screen) Tap: Next & Enter the device your adding: Tap: “Tank Module” or “Pump Module” Tap: Update Subscription 8. Tap: “Scan QR Code” (Sticker from inside of device) or manually enter the code. 9. Tap: “SAVE”- located top Right of screen. Device is now paired & ready to transmit data 10. Enter Site Information: Site Name, link a Tank Module or Make/Add to Group- (Multi site) 11. Tap: “Done” Then Tap “Start or Skip”: Tutorial. (3-step tutorial) 12. Tap: “I’m Ready” This will take you to home screen to select the site you just created 13. Locate & Tap on site: To view data 14. Set “Alert Thresholds”: Water Volume, PV- Voltage, Input Power & Input Current INSTALLATION 1. Module needs to be placed upright with an antenna pointing directly to the sky. 2. Please make sure that there is no metal, concrete or any other structures blocking the signal, this includes trees and buildings. 3. From the box, remove the module and the bag of screws 4. Carefully remove the lid from the base ensuring not to damage the cable termination. 5. Remove the pull-tab between the battery and the terminal, the unit is now ready to transmit. 6. Replace the lid and insert screws from the underside of the base. 7. Remove the mounting plate from the bottom of box 8. Feed the cable through the round hole on the top of the mounting plate 9. Fix the module to the mounting plate by: • Lifting the screw covers on the lid and inserting the bolts • Insert these bolts through the mounting plate and tighten the nuts 10. Screw the mounting plate to the underside of the solar frame through the three pre-drilled holes remembering that the cable is only 4m in length and needs to reach the CIU903 terminal connection point (self-tapping screws are not included). 11. Screw the antenna to the lid of the module 12. Route the cable back to the connection point of the CIU903 13. It is important to protect the cable from vermin and wildlife Pull Tab With Self Tappers Fix to underside of Solar Panel
Download PDF file
Cookie policy