INSTALLATION (15/MINS) Orientation: ONLY Mount the device vertically with a clear view to sky (fig.1) Antenna Area is: Top 1/3rd of module - Keep Above Metal Objects (fig.1) Nearby obstacles: Could obstruct transmission (Metal, Tree’s & Buildings) 1. Remove mounting plate/Cradle from device. (fig.2 Retaining Screw bottom) 2. Remove front cover (fig.2) then remove Pull Tab (fig.3) between battery and terminal. Device is now activated & ready to transmit data 3. Replace cover & slide on to bracket & re-insert retaining screw (fig.2) 4. Lower the prewired sensor to the bottom of tank (fig.4) Top 1/3 is Antenna Figure 1 Battery Compartment x2 AA L91 Lithium <3Yr Life Figure 3 PULL TAB Batteries replaceable from cradle (x4 screws) Screw or Cable Tie Cradle Figure 2 5M Sensor Cable Max Water Depth 3.5m Overflow Alert Figure 4 Float Level Actual Level Low Alert Level Sensor
Download PDF file
Cookie policy