“You can't control the temperature, you can't control the water quality very well” Ewen Leslie, Freshwater Engineering Manager at Scottish Sea Farms Read more about the Scottish Sea Farms case at grundfos.com The Scottish Sea Farms Barcaldine hatchery in the Scottish Highlands near Oban, UK. The situation Scottish Sea Farms – a land-and marine-based salmon farmer – used to operate its hatcheries with the “flow- through” water technique. They brought fresh water into their plants from nearby rivers or lakes, let it flow through their tanks and systems and then flow out again, back to the original water sources. This method posed a challenge, however. There was little control over what nature gives you. “You can't control the temperature, you can't control the water quality very well,” says Ewen Leslie, Freshwater Engineering Manager at Scottish Sea Farms Barcaldine atchery. For instance, inside the hatchery, the water must be 12°C (54°F). But incoming water temps in Scotland can swing wildly, depending on the season – as low as 2°C or as high as 20°C. The hatchery must thus spend a lot of resources heating or cooling the water. And that’s only one challenge – among several others relating to having control over a system that was increasingly unsustainable on different levels. Swinging temperatures and other factors also have the potential to stress the salmon, affecting growth. \ 02
Download PDF file
Cookie policy